Interrupt handerler issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt handerler issue

1,288 Views
vignesh70
Contributor I

Hai, 

 

|------------|                                                   |------------|

|------------| Gpio ---------------------->PTC0    |------------| (Wating for Faling Edge) (Ext Interrupt)                                                         

Salve Device                                              Master Device(K32L Series Controller)   

 

 

Currently am Facing the issue Read the interrupt Signal but our Controller not Capture the interrupt signal ,but we are Probe the Interrupt line Via CRO Slave Device generate the Interrupt signal But Our Microcontroller not capture the interrupt signal. and Timer 2 Also we Configure but That also Not set the status Bit so its not go for the handler function. main issue is the interrupt status Register is Not set at get the interrupt signal. so our IDE is not go for the Handler functions. actually Your Suspecting on the Firmware configuration side but Same Code we are interface with Same controller and same pin Configuration hardware That time is Working properly, But Both are Different Sematic, Run on Same Range Crystal oscillator. At the time we are suspecting the hardware side, the hard ware is done the Same interrupt  pin  done the digital Read and Write also 

 

Main Issue: Any interrupt its get not Set the Status bit so our Ide not  execute the  interrupt handler but firmware side is fine and Hardware also fine 

 

 

Thanks and regards,

Vignesh kumar M 

 

 

 

 

0 Kudos
Reply
0 Replies