FB Clock Output not rectangular

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FB Clock Output not rectangular

Jump to solution
4,838 Views
Kolibri
Contributor III

Hello i´m working with the Development Board FRDMK32L3A6 and i want to use the FB_CLKOUT Pin to clock another Board. Here in this pictures are the settings i use.

Clock_Diagram_FRDMK32L3A6.png

Clock_Pin_FRDMK32L3A6.png

Now i´ve measured the Clock Signal with an Oscilloscope and this is what i get. Am i doing something wrong on my measurement or does the clock signal look like this? How can i change it to be rectangular?

CLOCK.png

Thanks and best regards

Tags (1)
0 Kudos
Reply
1 Solution
4,801 Views
Kolibri
Contributor III

The clock signal never looks like a perfect squarewave and it works fine like it is.

Best regards Kolibri

View solution in original post

0 Kudos
Reply
3 Replies
4,829 Views
Kolibri
Contributor III

I think i got it, i have to add a series resistor to the signal i will try it tomorrow.

0 Kudos
Reply
4,824 Views
Kolibri
Contributor III

I´ve tried now with different resistors, the signal changes but it´s not gettin rectangular. Can someone please help me to solve this problem. Is there a formula to calculate the series resistor or is it even needed?

Thanks and best regards

0 Kudos
Reply
4,802 Views
Kolibri
Contributor III

The clock signal never looks like a perfect squarewave and it works fine like it is.

Best regards Kolibri

0 Kudos
Reply