PROFINET-RT: Enable Callback Indication for cyclic IO - data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PROFINET-RT: Enable Callback Indication for cyclic IO - data

PROFINET-RT: Enable Callback Indication for cyclic IO - data

Note-1 : Using this callback routine can have a massive influence to the real time behavior of the stack!

Note-2 : This feature is unavailable for multicore projects until GOAL v2.23.0.

The example below shows the use of the callback function:

  • Create the following local prototype and variables

  • Add the callback function to the callback handler

/****************************************************************************/
/* Local Prototypes */
/****************************************************************************/
static GOAL_STATUS_T appl_pnioCb(
GOAL_PNIO_T *pHdlPnio, /**< PROFINET instance */
GOAL_PNIO_CB_ID_T id, /**< callback id */
GOAL_PNIO_CB_DATA_T *pCb /**< callback parameters */
);


/****************************************************************************/
/* Local Variables */
/****************************************************************************/
static GOAL_BOOL_T flgAppReady = GOAL_FALSE; /**< app ready flag */
static GOAL_PNIO_AR_ID_T idAr = 0; /**< AR ID */
static GOAL_PNIO_T *pPnio; /**< PROFINET instance */
static char targetData[APPL_MOD_SIZE]; /**< dummy where data is copied to */


/****************************************************************************/
/** Profinet Callback Handler
*
* This function collects all callbacks from the stack and decides if the
* callback must be handled.
*/
static GOAL_STATUS_T appl_pnioCb(
GOAL_PNIO_T *pHdlPnio, /**< PROFINET instance */
GOAL_PNIO_CB_ID_T id, /**< callback id */
GOAL_PNIO_CB_DATA_T *pCb /**< callback parameters */
)
{
GOAL_STATUS_T res = GOAL_OK; /* return value */

UNUSEDARG(pHdlPnio);

/* handle callback IDs */
switch (id) {

case GOAL_PNIO_CB_ID_APPL_READY:
/* application ready was confirmed, start data handling if not
* already running */
if (GOAL_TRUE != flgAppReady) {
flgAppReady = GOAL_TRUE;
idAr = pCb->data[0].idAr;
}
break;

case GOAL_PNIO_CB_ID_RELEASE_AR:
/* AR was released, stop data handling if it was the first AR */
if (idAr == pCb->data[0].idAr) {
flgAppReady = GOAL_FALSE;
idAr = 0;
}
break;

case GOAL_PNIO_CB_ID_BLINK:
goal_targetSetLeds((pCb->data[1].stateDcpLight) ? UINT32_MAX : 0);
break;

case GOAL_PNIO_CB_ID_NEW_IO_DATA:
/* New I/O data received.
* Be careful: this call will block the PNIO stack
* so just do the copying here and nothing else.
* If not fast enough, just set a flag and retrieve the data
* later in appl_loop if required.
**/
memcpy(targetData, pCb->data[2].pCu8, pCb->data[1].u16);
break;
default:
break;
}

return res;
}

 

To use the cb function GOAL_PNIO_CB_ID_NEW_IO_DATA, the following functions have to be called exactly in the order described below before and after function goal_pnioNew(...):

  • goal_pnioCfgNewIoDataCbSet(GOAL_TRUE); → configure stack to feature the GOAL_PNIO_CB_ID_NEW_IO_DATA callback

  • goal_pnioCyclicCtrl(pPnio,GOAL_TRUE); → enable GOAL_PNIO_CB_ID_NEW_IO_DATA callback for each arrived cyclic frame

/****************************************************************************/
/** Application Setup
*
* Setup the application.
*/
GOAL_STATUS_T appl_setup(
void
)
{
GOAL_STATUS_T res; /* result */

/* configure stack to feature the GOAL_PNIO_CB_ID_NEW_IO_DATA callback */
goal_pnioCfgNewIoDataCbSet(GOAL_TRUE);

/* create new PROFINET instance */
res = goal_pnioNew(&pPnio, APPL_PNIO_ID, appl_pnioCb);
if (GOAL_RES_ERR(res)) {
goal_logErr("failed to create a new PROFINET instance");
return res;
}

/* enable GOAL_PNIO_CB_ID_NEW_IO_DATA callback for each arrived cyclic frame */
goal_pnioCyclicCtrl(pPnio,GOAL_TRUE);

goal_logInfo("Initializing device structure");

/* from here create the device configuration */
...

/* PROFINET configuration succesful */
goal_logInfo("PROFINET ready");

return GOAL_OK;
}
标签 (3)
无评分
版本历史
最后更新:
‎09-23-2025 08:03 AM
更新人: