The Test Case TF-1200[4][10] "#49 Op > SafeOp, WD expired“ gives a warning if the device uses GOAL and a multicore architecture over SPI. This is due to time consuming remote procedere calls (RPC) leading to delayed watchdog timeouts, which are not triggered within the defined timeout of WD-time + 10% WD-time.
A warning does not result in a failed conformance test.