EtherCAT Application Examples: GOAL Application description

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EtherCAT Application Examples: GOAL Application description

EtherCAT Application Examples: GOAL Application description

Introduction

 

NXP EtherCAT stack provides different sample applications for GOAL. These applications have been created with help of Industrial Communication Creator and show how to setup and use the stack. The next chapter lists all application examples, which are located at appl/goal_ecat/. Related projects are placed at projects/goal_ecat* next to edt sub-directory ICC projects, EEPROM binaries and XML-device description files used by EtherCAT software like TwinCAT or Ethernet Codesys Master PLC for interacting with the device.

ECAT projects are organized into single-/ multi-core and full-source/ demo projects:

projects/goal_ecat - full source projects
projects/goal_ecat_lib - 1h demo library projects
projects/goal_ecat_rpc - multi-core projects
projects/goal_ecat_rpc_lib - 1h demo library projects for multi-core projects

Application description

 

All listed applications can be used for single and multi-core platforms equally. Only exception is 00_rpc_cc, which is designed for the communication core of multi-core platforms.

In goal_appl.c is the initialization of GOAL and the EtherCAT stack located. The behavior of the sample application is controlled by goal_app_ecat.c, while the object dictionary is created by goal_appl_ecat_objects.c. Some additional, application specific files may be placed in the directories. Please note the file description of the related file for further information.

appl/goal_ecat/00_rpc_cc

 

This application must be run on the communication core of a device. It provides the functionality for all other examples to the application core. It is not restricted to the examples but also provides the full GOAL EtherCAT functionality to the user application.

The EtherCAT demo projects/00_goal_rpc_demo/ is a 1h time limited, full feature protocol stack library.

appl/goal_ecat/01_simple_io

 

This application is a simple example of handling IOs. It features FoE and CoE and is configured by an explicit device ID APPL_ECAT_EXPL_DEV_ID of 5.

Following objects are mapped as I/O data and can be accessed from a PLC (e.g. TwinCAT or Ethercat Codesys Master PLC).

Object ID Variable Name Description

0x6000:0x01

applU8ButtonInput

8 byte: button input

0x6120:0x01

applVarU32Input

32 byte: input mirror data

0x6200:0x01

applU8LedOutput

8 byte: LED output

0x6320:0x01

applVarU32Output

32 byte: output mirror data

 

appl/goal_ecat/02_eoe_http

 

This application is equal to appl/goal_ecat/01_simple_io expanded by EoE feature.

The file goal_appl.c contains a simple webserver content, which can be accessed via EoE at port APPL_TCP_PORT (8081) of device’s IP. Up to APPL_HTTP_CHAN_CNT (4) HTTP channels are available.

 
 
标签 (3)
无评分
版本历史
最后更新:
‎09-24-2025 09:18 AM
更新人: