TJA1085G VBUF Supply

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TJA1085G VBUF Supply

跳至解决方案
2,037 次查看
Mayur_M_Bharadwaj
Contributor II

Dear team,

For TJA1085G, is it mandatory to connect VBUF to 5V Supply, or is it optional? InAH1001 Document, 

  • In Section 4.1.2, it says VBUF is derived from VCC/VBAT
  • In Fig 27, there is no 5V connection to VBUF
  • In Fig 28, there is 5V connection to VBUF

If it is internally derived, we wanted to understand why it is connected in Fig 28. We do not have Wake-Up Requirement, and VBAT and VCC will be connected to 5V. So, we wanted to understand the connection of VBUF to 5V externally.

 

Thank you!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,023 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Mayur,

Figure 27 shows a system with wake-up support, where VBUF is separated and connected to a capacitor (CBUF) to allow wake-up signaling even when VCC is off.

Figure 28 shows a system without wake-up support, where VBAT, VCC and VBUF are all tied together to 5V. This simplifies the design and is acceptable when wake-up functionality is not needed.

So in your case, you can connect VBUF directly to 5V and you do not need a separate supply or buffer capacitor.

BRs, Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,024 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Mayur,

Figure 27 shows a system with wake-up support, where VBUF is separated and connected to a capacitor (CBUF) to allow wake-up signaling even when VCC is off.

Figure 28 shows a system without wake-up support, where VBAT, VCC and VBUF are all tied together to 5V. This simplifies the design and is acceptable when wake-up functionality is not needed.

So in your case, you can connect VBUF directly to 5V and you do not need a separate supply or buffer capacitor.

BRs, Tomas

0 项奖励
回复
1,997 次查看
Mayur_M_Bharadwaj
Contributor II

Hello Tomas,

Thanks for the feedback.

0 项奖励
回复