How to distinguish CAN L / CAN H OPEN using TJA1442AT ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to distinguish CAN L / CAN H OPEN using TJA1442AT ?

Jump to solution
1,105 Views
mumumilmil
Contributor II

Hi, I'm using TJA1442AT CAN IC to Automotive HS_CAN BUS.

If CAN High or CAN Low have OPEN, TJA1442 IC detects that OPEN?

- OPEN : Ex) Circuit short/open

Thanks.

Tags (1)
0 Kudos
Reply
1 Solution
1,080 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The TJA1442AT does not detect or report an “OPEN” (disconnected) CANH or CANL condition. It has no diagnostics for open-load conditions on the bus lines.

BRs, Tomas

 

View solution in original post

0 Kudos
Reply
2 Replies
1,081 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The TJA1442AT does not detect or report an “OPEN” (disconnected) CANH or CANL condition. It has no diagnostics for open-load conditions on the bus lines.

BRs, Tomas

 

0 Kudos
Reply
1,064 Views
mumumilmil
Contributor II

Thanks.

Then, S32K144W can detects CAN BUS OFF?

Tags (1)
0 Kudos
Reply