NVT4858 for QSPI voltage level translation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVT4858 for QSPI voltage level translation

1,170 Views
vjen
Contributor I

The NVT4858 is designed for SD and SIM application. Can I use it for QPSI?

My circuit:

Host side: 1.2V QSPI, SCLK is up to 50 MHz

Flash memory: 3.3V QSPI

Please advise. Thanks.

Labels (2)
0 Kudos
Reply
1 Reply

1,159 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Vance,

please refer to the NVT4858 datasheet. Yes, the NVT4858 fulfills your requirements. 

The NVT4858 is designed for SD and SIM application. Can I use it for QPSI?

JozefKozon_0-1748321478169.png

Host side: 1.2V QSPI, SCLK is up to 50 MHz

JozefKozon_1-1748321553242.pngJozefKozon_2-1748321581043.png

Flash memory: 3.3V QSPI

JozefKozon_3-1748321614567.png

With Best Regards,

Jozef