LPC-Link2 used in keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 used in keil

452 Views
just_lee
Contributor II

I would like to work on LPC55S14 MCU using LPC-Link2 in keil5.
However, Keil5 says that they can't find LPC-link2.

just_lee_0-1756952321595.png

To address this issue, I downloaded LPCScrypt and ran "Program LPC-Link2 with CMSIS-DAP_2.1.3_83" and updated LPCK-LINK2.

just_lee_1-1756952488444.png

After the update, LPC-link2 will be displayed as "LPC-LINK2 UCom Port (COM15)" in Device Manager as shown above.

But I still can't find LPC-Link2 on Keil5.
What are the options to solve this problem?

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

431 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @just_lee 

Thank you for contacting us.
Please update the CMSIS-DAP firmware of your LPC-Link2 to the J-Link firmware, then check if it can be recognized by KEIL.

 

BR

Alice

0 Kudos
Reply

416 Views
just_lee
Contributor II

Thank you for your answer.

 

just_lee_0-1757026628413.png

 

As you said, I updated LPC-Link2 to J-Link using "Program LPC-Link2 with Segger J-Link_2.1.3_83".

After that, when I checked from Keil5 to JLink, it seems to have been recognized as follows.

But the MCU I'm using is a SWD environment, so I want to use "CMSIS-DAP", is there a solution?

 

0 Kudos
Reply

351 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @just_lee 

How about change JTAG to SWD:

Alice_Yang_0-1757404799916.png

 

BR

Alice

 

 

 

0 Kudos
Reply