To dumb on a TFT disply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To dumb on a TFT disply

3,898件の閲覧回数
sajithdevidas
Contributor III

the examples from gui guider is perfectly working on the rt1170 evk board , but im having the same board with an another display(RGB TFT Display (800*480)), what changes i have to made in the current working code which is suitable for the on-board display of evk board

 

0 件の賞賛
返信
1 返信

3,870件の閲覧回数
zongchunyu
NXP Employee
NXP Employee

Hello sajithdevidas,

you can create a project using the custom panel like screenshot1, then go to the <project folder>\sdk\Core\board folder and edit the display_support.c/h file to add display config for your panel like screenshot2.

 

Best Regards

Zongchun

0 件の賞賛
返信