Regarding image format issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding image format issues

1,730 Views
ZackLin
Contributor I

GUI Guider only offers two image format options, both of which occupy a large amount of space. Some of my images are only two-color and require smaller format options, such as the variety of image formats provided in the link   https://lvgl.io/tools/imageconverter.  

0 Kudos
Reply
3 Replies

1,687 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @ZackLin 

Please Use the V9 project. 

Harry_Zhang_0-1765350532880.png

If this doesn't meet your needs, you can only manually add it to the code.

BR

Harry

 

0 Kudos
Reply

1,321 Views
ZackLin
Contributor I

ZackLin_0-1767063633495.png

Will guiGuider support more image formats in the future? The current formats are too limited, which is not ideal for small-capacity devices. For example, could support for the "CF_INDEXED_2_BIT" format be added?

0 Kudos
Reply

1,320 Views
ZackLin
Contributor I
I'm using the v8 version of the project.
0 Kudos
Reply