RDK Demo Controller Target Detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RDK Demo Controller Target Detection

1,744 Views
Paroz
Contributor III

Hello everyone,

I'm trying to make an SDK DEMO example but I can't see anything in the Radar Demo Controller Guide. As you can see in picture successfully connecting but it doesn't see any target. 

What I did to fix this problem;

- I checked the IP adress and follow to instructions in FIRST_Quick Start Guide for RDKS32R274

- I thought that may be  it causes from Defender Firewall so I disabled the firewall. 

- There is a one sentences in this Start Guide document. Which is "The back panel may be removed and if the system is on, you should see solid light from LEDs on the boards reflecting off the case."

The 4 LEDs above are working and giving yellow light but The LED below is red.  

WhatsApp Image 2022-11-23 at 2.59.08 PM.jpeg

I want to be sure so I am asking, which one Do I have to select for successfully connection between S32DS and RDK

ASK.png

Other important parameters ; Capture.PNG

ekle.png

I tried the all options but I didn't obtain affirmative result. How can I solve this problem ? If you give suggesiton or idea no doubt I am glad. 

Btw I see the ethernet light blinking when debugging the code

rdk.png

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Output ;

output.png

0 Kudos
Reply
0 Replies