LPC55S69 Configtool SAMPLE project, with LvGL GUIGuider UI and ILI9341 and EC11 Rotary Encoder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 Configtool SAMPLE project, with LvGL GUIGuider UI and ILI9341 and EC11 Rotary Encoder

3,972件の閲覧回数
gertvb
Contributor III

Hallo Everyone!

https://github.com/gertvb/LPC55S69_GuiGuider

 

An MCUXpresso SAMPLE project where I've done the setup for the LPC55S69 with Configtools, and

combined it with a simple LVGL UI generated by GUIGuider

 

Hardware :

WaveShare 2.4inch tft with ILI9341

EC11 rotary encoder, debounced in software 

 

Configtools:

SPI-DMA

PINT

GPIO

 

Hope it is of help to someone

 

Regards

Gert

A TechExplorer working with Embedded Software and Electronics in Agriculture and Alternative Energy
2 返答(返信)

3,866件の閲覧回数
zhenhualuo
NXP Employee
NXP Employee

Hi Gert, 

Thanks for your sharing.

LPC55S69 is supported by GUI Guider v1.2.0 which is available on  http://nww.preview.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER. 

 

Best Regards, 

Zhenhua 

3,907件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Hi Gert,

Many thanks for sharing your project with the community.

I did notice in your github docs that you query whether Edgeline is GUI Guider. These are separate tools that are being developed completely independently; the LVGL.io tool is developing Edgeline as a premium tool to complement its design service offerings and currently has a beta version out. GUI Guider was developed by NXP as a free tool for our customers.

We work closely with the LVGL.io team (we used their services to develop some of the graphics in the demos you can see on nxp.com) and see these choices as beneficial to our customers; you'll see us promoting Edgeline too as we are big believers in LVGL!

Best regards,

Brendon

0 件の賞賛
返信