How to compile gui guider project as dll

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to compile gui guider project as dll

1,249件の閲覧回数
bosnian_beast
Contributor III

I have to import gui guider project in an mcuxpresso project. I now have a complicated procedure that utilizes python script to copy necessary files to the project. It would be very useful to me if I could compile the gui guider project as a dll and then simply include it in my project. 

This can also be useful if I have multiple gui's, where I can flash multiple dll's and then the app will load them on runtime based on which gui is needed. 

In case that it isn't possible now to do it, I would like to make an appeal to include this funcitonality in the next version.

0 件の賞賛
返信
1 返信

1,219件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @bosnian_beast,

This is not possible on the current version of GUI Guider, but I will relay your suggestion to the GUI Guider team in order for them to discuss and hopefully add on a future release of the Tool. It would be a great thing to add to GUI Guider.

BR,
Edwin.

0 件の賞賛
返信