Guider 1.5 is installed on widows11, the first time the simulator runs normally,but the second JAVA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Guider 1.5 is installed on widows11, the first time the simulator runs normally,but the second JAVA

2,434 Views
Lujiantu0926
Contributor I
Cleaning Generate image files......
Cleaning Generate screen files......

Converting fonts......

Running UIT To Generate Code

'java' �����ڲ����ⲿ���Ҳ���ǿ����еij��� ���������ļ���

 

 

0 Kudos
Reply
2 Replies

2,401 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Lujiantu0926 

Sorry we haven't tested on Windows11. 

You can try to Install Java Runtime Environment refer to <GUI_Guider_User_Manual>->2.3.1 Install Java Runtime Environment.

 

BR

Alice

 

0 Kudos
Reply

2,336 Views
zhenhualuo
NXP Employee
NXP Employee

Hi @Lujiantu0926,

Have you checked the JAVA installation on your machine? Does GUI Guider work normally now? You can run java command directly in cmd.exe of Windows to check if openjdk is installed correctly. 

 

Best Regards, 

Zhenhua

0 Kudos
Reply