GUI guider compile error:'SDL2/SDL.h' file not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI guider compile error:'SDL2/SDL.h' file not found

6,115 Views
richen
Contributor I

How to figure out the compile error : 'SDL2/SDL.h' file not found

Use MAC OS 12.6 and latest guy guider version.

0 Kudos
Reply
5 Replies

6,102 Views
LiubinGong
NXP Employee
NXP Employee

Hi  richen

  Is your computer architecture arm64?  In response to this problem, I suggest that you can install SDL with source code. Please ensure the install path is /usr/local.  Since the current version is not yet supported by M-core laptops, Some functions will have problems. it's predictable. BTW, We will officially support the ARM64 M-core Mac laptop in the next release(1.6.0). 

BR

Liubin

0 Kudos
Reply

5,539 Views
application_ninja
Contributor V

Any update on this? Still a problem on Gui Guider 1.6.1 with a M-Core Mac...

0 Kudos
Reply

5,530 Views
LiubinGong
NXP Employee
NXP Employee

Hi @application_ninja 

 Please install the SDL based on the steps:

Capture.PNG

Thanks

Liubin

3,462 Views
lizm0712
Contributor I
it useful,thanks!
0 Kudos
Reply

5,511 Views
application_ninja
Contributor V

This worked, thank you!

0 Kudos
Reply