GUI-Guider support for other NXP boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI-Guider support for other NXP boards

2,278 Views
krestic
Contributor I

Hello,

I am using GUI-Guider-1.7.2 on Windows. Currently there is only one template for the i.MX9 series when you choose LVGL version 8.3.10. Is there a way I could add my own template to the i.MX category, e.g. for previous i.MX series?

 

Best regards

0 Kudos
Reply
3 Replies

2,258 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @krestic,

I'm afraid this is not possible, as the i.MX93 is the only MPU supported by GUI Guider, as shown on the "Supported Devices" list of the product page:

EdwinHz_0-1718396757445.png

BR,
Edwin.

2,221 Views
krestic
Contributor I

Does this also imply that it's not possible to create custom templates?

0 Kudos
Reply

2,211 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @krestic,

It is not possible to create custom templates for boards that are not supported by GUI Guider. Sorry for the inconvenience this may cause.

BR,
Edwin.

0 Kudos
Reply