Freemaster connection failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster connection failed

1,505 Views
VARSHA_PRIYADARSINI
Contributor II

When I try to link freeMASTER to bind the variables, i get an error called "Failed to link FreeMASTER, please check IP and port!" 

In link config:

Address: localhost

Port: 41000

 

Can someone explain why this is happening and how to link freeMASTER in gui guider

0 Kudos
Reply
1 Reply

1,490 Views
LiubinGong
NXP Employee
NXP Employee

Hello @VARSHA_PRIYADARSINI 

    Thanks for your feedback,  First you need to open the FreeMaster IDE, then link the server in GUI Guider. If you have opened multiple Freemaster instances, select the corresponding port number. Please find more information from FreeMASTER debug steps.  Hope this helps.

Best Regards

Liubin

0 Kudos
Reply