Bug in font generation in V18.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug in font generation in V18.0?

1,672件の閲覧回数
TsuyoshiSugiyama
Contributor II

When generating fonts in V18.0, the font height changes.
For example, when creating a font with a height of 24px, the height has changed to 29px.
This makes it impossible to use the UI I have created so far.
Is this a bug? Even if it is a specification, it is still a problem.

TsuyoshiSugiyama_0-1723188652647.png

 

0 件の賞賛
返信
2 返答(返信)

1,654件の閲覧回数
Alphabert_Liu
NXP Employee
NXP Employee

Dear @TsuyoshiSugiyama ,

29 here refers to the line height, which refers to the height of a line of text, including the height of the characters themselves and the line spacing.If you want, you can reduce the font line spacing.

Best Regard

Liu

0 件の賞賛
返信

1,530件の閲覧回数
TsuyoshiSugiyama
Contributor II

Thank you for your answer.
How can I reduce the line spacing of the font?
We designed the UI at 24px, so there are problems if that is changed.

Best Regard

0 件の賞賛
返信