freemaster with s32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freemaster with s32

1,946 Views
wwq1
Contributor I

我使用S32 design studio for s32 platform 3.5安装freemaster,但是显示 could not find jar:file:freemaster_s32k3_v3.0zip,请问是为什么呢?

0 Kudos
Reply
1 Reply

1,872 Views
iulian_stan
NXP Employee
NXP Employee

Hi @wwq1,

We provide 2 archives with FreeMASTER Driver. One is the plain archive with the source code and the second one is packaged as Eclipse Update Site. Could you make sure that you use the later version. It is highlighted in the picture bellow:


1.png1.png

 

Then  you can follow the steps as in the following print screen to install the update site from within S32DS:

2.png2.png

 

If that does not work, please let us know at what step does is fails.

0 Kudos
Reply