could not install freemaster lite in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

could not install freemaster lite in linux

11,918 Views
yjy
Contributor I

__________________________________________________________________________

Tue Aug 27 07:52:43 CST 2024

Free Memory: 18322 kB
Total Memory: 39936 kB

java.class.path:
/tmp/install.dir.88991/InstallerData
/tmp/install.dir.88991/InstallerData/installer.zip

ZGUtil.CLASS_PATH:
/tmp/install.dir.88991/InstallerData
/tmp/install.dir.88991/InstallerData/installer.zip

sun.boot.class.path:
<none specified>

java.ext.dirs:
<none specified>

java.version == 22.0.2 (Java 2+)
java.vm.name == OpenJDK 64-Bit Server VM
java.vm.vendor == Arch Linux
java.vm.version == 22.0.2+9
java.vm.specification.name == Java Virtual Machine Specification
java.vm.specification.vendor == Oracle Corporation
java.vm.specification.version == 22
java.specification.name == Java Platform API Specification
java.specification.vendor == Oracle Corporation
java.specification.version == 22
java.vendor == Arch Linux
java.vendor.url == https://openjdk.org/
java.class.version == 66.0
java.library.path == /usr/java/packages/lib:/usr/lib64:/lib64:/lib:/usr/lib
java.compiler == null
java.home == /usr/lib/jvm/java-22-openjdk
java.io.tmpdir == /tmp
os.name == Linux
os.arch == amd64
os.version == 6.10.6-zen1-1-zen
path.separator == :
file.separator == /
file.encoding == UTF-8
user.name == yjy
user.home == /home/yjy
user.dir == /tmp/install.dir.88991
user.language == en
user.region == null
__________________________________________________________________________

Installed Feature(s) FMSTR Lite, FMSTR NM of FreeMASTER Lite 1.3.0

Install Begin: AUGUST 27, 2024 7:51:42 PM CST
Install End: AUGUST 27, 2024 7:52:39 PM CST

Installed by InstallAnywhere 20.0 Premier Build 6336


User Interactions
-----------------


#Choose Product Features
#-----------------------
CHOSEN_FEATURE_LIST=FMSTR Lite,FMSTR NM
CHOSEN_INSTALL_FEATURE_LIST=FMSTR Lite,FMSTR NM
CHOSEN_INSTALL_SET=FL

#Choose Install Folder
#---------------------
USER_INSTALL_DIR=/home/yjy/NXP/FreeMASTER Lite 1.3.0

#Choose Link Folder
#------------------
USER_SHORTCUTS=/home/yjy/Desktop/FreeMASTER Lite 1.3.0

#Install
#-------
-fileOverwrite_/tmp/029557.tmp/FNPLicense/license.jar=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/cll/x64/FnpCommsSoap.so=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/cll/x64/libclljni.so=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/cll/x64/libcll_app.so=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/cll/x64/libcll_app_libFNP.so=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/cll/x64/libcll_svr.so=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/cll/x64/libcll_svr_libFNP.so=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/FNPLicensingService/FNPLicensingService=Yes
-fileOverwrite_/tmp/029557.tmp/FNPLicense/install_fnp.sh=Yes

Summary
-------

Installation: Unsuccessful.

25 Successes
14 Warnings
1 NonFatalErrors
1 FatalErrors

Action Notes:

None

Install Log Detail:

Check Disk Space: /home/yjy/NXP/FreeMASTER Lite 1.3.0
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:316,257,981 Bytes Free Disk Space:342,098,677,760 Bytes

Check Disk Space: /home/yjy/NXP/FreeMASTER Lite 1.3.0
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:316,257,981 Bytes Free Disk Space:342,098,677,760 Bytes

Check Disk Space: /home/yjy/NXP/FreeMASTER Lite 1.3.0
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:316,257,981 Bytes Free Disk Space:342,098,640,896 Bytes

Install Directory: /tmp/029557.tmp/
Status: SUCCESSFUL
Additional Notes: NOTE - Directory already existed

Install Directory: /tmp/029557.tmp/FNPLicense/
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/license.jar
Status: SUCCESSFUL

Install Directory: /tmp/029557.tmp/FNPLicense/cll/
Status: SUCCESSFUL

Install Directory: /tmp/029557.tmp/FNPLicense/cll/x64/
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/cll/x64/FnpCommsSoap.so
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/cll/x64/libclljni.so
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_app.so
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_app_libFNP.so
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_svr.so
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_svr_libFNP.so
Status: SUCCESSFUL

Install Directory: /tmp/029557.tmp/FNPLicense/FNPLicensingService/
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/FNPLicensingService/FNPLicensingService
Status: SUCCESSFUL

Install File: /tmp/029557.tmp/FNPLicense/install_fnp.sh
Status: SUCCESSFUL

Execute Script/Batch file: Install Flexera service
Status: SUCCESSFUL


Execute Command: java "-Djava.library.path=/tmp/029557.tmp/FNPLicense/cll/x64" -jar "/tmp/029557.tmp/FNPLicense/license.jar" verify -feature Activated -version 1.3 -prod FreeMASTER_Lite_1.3.RTM
Status: SUCCESSFUL

Execute Command: java "-Djava.library.path=/tmp/029557.tmp/FNPLicense/cll/x64" -jar "/tmp/029557.tmp/FNPLicense/license.jar" run -feature Activated -version 1.3 -prod FreeMASTER_Lite_1.3.RTM
Status: SUCCESSFUL


Install Uninstaller: FreeMASTER Lite 1.3.0(Install All Uninstaller Components)
Status: SUCCESSFUL

Install Directory: /home/yjy/NXP/FreeMASTER Lite 1.3.0/_FreeMASTER_Lite_installation/InstData/
Status: SUCCESSFUL

Install Uninstaller: FreeMASTER Lite 1.3.0(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall File: /home/yjy/NXP/FreeMASTER Lite 1.3.0/_FreeMASTER_Lite_installation/Logs/FreeMASTER_Lite_1.3.0_Install_08_27_2024_19_52_07.log
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/license.jar
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/cll/x64/FnpCommsSoap.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/cll/x64/libclljni.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_app.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_app_libFNP.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_svr.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/cll/x64/libcll_svr_libFNP.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/FNPLicensingService/FNPLicensingService
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: /tmp/029557.tmp/FNPLicense/install_fnp.sh
Status: WARNING
Additional Notes: WARNING - The file does not exist


Status: SUCCESSFUL

Uninstall Folder: /tmp/029557.tmp/FNPLicense/cll/x64
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: /tmp/029557.tmp/FNPLicense/cll
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: /tmp/029557.tmp/FNPLicense/FNPLicensingService
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: /tmp/029557.tmp/FNPLicense
Status: WARNING
Additional Notes: WARNING - The path does not exist

Error occurred while installing the following Action, hence rolling back the installation....!


Action Name: Trigger Rollback Action
Action Description: Trigger Rollback Action


Error Details as below:


This action rolls back the Installation.

0 Kudos
Reply
23 Replies

1,141 Views
iulian_stan
NXP Employee
NXP Employee

A possible workaround I could think of is installing FreeMASTER Lite on another Workstation or a Virtual Machine and copy the binaries from the guest (secondary) machine to your main (host) machine. 

The only dependency that is required is the licensing service that according to your logs was installed successfully (you can find it in /usr/local/share/FNP/service64/11.13.0/FNPLicensingService).
It should persist even if the installation fails.

Note: when running FreeMASTER Lite you may need to add license folder from FreeMASTER Lite directory to LD_LIBRARY_PATH.

0 Kudos
Reply

1,623 Views
yjy
Contributor I
yeah, I wrote the license , and then rolled back, by the way , I am using arch linux
0 Kudos
Reply

1,587 Views
yjy
Contributor I
yeah, I have introduced my root password and run `export LAX_DEBUG=true`, but it still rolled back
```
No of blocks of size 8192 to extract for custom unix file : 1
Extracting locale bundle from ./FMASTERL13.bin to /home/yjy/Downloads/custom_padded ...
Extracting done, exit code = 0
Extracting locale bundle from /home/yjy/Downloads/custom_padded to /home/yjy/Downloads/custom ...
Extracting done, exit code = 0
Preparing to install
Checking for POSIX df.
Found POSIX df.
Checking tail options...
Using tail -n 1.
True location of the self extractor: /home/yjy/Downloads/FMASTERL13.bin
Creating installer data directory: /tmp/install.dir.38823
Creating installer data directory: /tmp/install.dir.38823/InstallerData
Gathering free-space information...
Space needed to complete the self-extraction: 11410 blocks
Available space: 15239024 blocks
Available blocks: 15239024 Needed blocks: 11410 (block = 512 bytes)
This installation does not contain a VM.
Extracting the installation resources from the installer archive...
Extracting install.zip from ./FMASTERL13.bin to /tmp/install.dir.38823/InstallerData/installer.zip ...
Extracting to padded done, exit code = 0
Extracting from padded to zip done, exit code = 0
Creating disk1 data directory: /tmp/install.dir.38823/InstallerData/Disk1
Creating instdata data directory: /tmp/install.dir.38823/InstallerData/Disk1/InstData
Extracting resources from ./FMASTERL13.bin to /tmp/install.dir.38823/InstallerData/Disk1/InstData/Resource1.zip ...
Extracting done, exit code = 0
Configuring the installer for this system's environment...

========= Analyzing UNIX Environment =================================
Setting UNIX (linux) flavor specifics.
Importing UNIX environment into LAX properties.
Checking for POSIX awk.

========= Analyzing LAX ==============================================
LAX found............................ OK.
LAX properties read.................. OK.

========= Finding VM =================================================
Valid VM types.......................... 1.7+
Expanded Valid VM types................. 1.7+
Found jvmspecs.properties
JVM Spec Build Option Specified Without VM
Searching without JVM specs
Searching without JVM specs
WARNING! No valid lax.nl.current.vm available.
/usr/xpg4/bin:/usr/local/sbin:/usr/local/bin:/usr/bin:/bin:/usr/bin:/sbin:/usr/sbin:/usr/local/bin
Searching for VMs in PATH:
Looking in:............................. /usr/xpg4/bin
Looking in:............................. /usr/local/sbin
Looking in:............................. /usr/local/bin
Looking in:............................. /usr/bin
Found VM:............................. /usr/bin/java
Version:............................. 22.0.2
Looking in:............................. /bin
Found VM:............................. /bin/java
Version:............................. 22.0.2
Looking in:............................. /usr/bin
Found VM:............................. /usr/bin/java
Version:............................. 22.0.2
Looking in:............................. /sbin
Found VM:............................. /sbin/java
Version:............................. 22.0.2
Looking in:............................. /usr/sbin
Found VM:............................. /usr/sbin/java
Version:............................. 22.0.2
Looking in:............................. /usr/local/bin
checking: "22.0.2" against "1.7+": passed
* Using VM:............................. /usr/lib/jvm/default-runtime/bin/java
Inspected VM version -> 22.0.2
Using VM version -> 22.0.2
Java 9 or higher version detected. Adding module access switch.

========= Virtual Machine Options ====================================
LAX properties incorporated............. OK.
classpath............................... "/tmp/install.dir.38823/InstallerData:/tmp/install.dir.38823/InstallerData/installer.zip"
main class.............................. "com.zerog.ia.installer.Main"
.lax file path.......................... "/tmp/install.dir.38823/temp.lax"
user directory.......................... "/tmp/install.dir.38823"
stdout to............................... "console"
sterr to................................ "console"
install directory....................... ""
JIT..................................... none
option (verify)......................... off
option (verbosity)...................... none
option (garbage collection extent)...... none
option (garbage collection thread)...... none
option (native stack max size).......... none
option (java stack max size)............ none
option (java heap max size)............. 50331648
option (java heap initial size)......... 16777216
option (lax.nl.java.option.additional).. -Dlax.debug.level=4 -Dlax.debug.all=true -Djdk.util.zip.disableZip64ExtraFieldValidation=true
option (Java 9 and above switch)........ --add-opens java.base/jdk.internal.loader=ALL-UNNAMED -Dsun.java2d.uiScale.enabled=false

========= Display settings ===========================================
./FMASTERL13.bin: line 3652: hostname: command not found
X display............................... local
UI mode................................. gui

Launching installer...

========= VM Command Line ============================================
options: --add-opens java.base/jdk.internal.loader=ALL-UNNAMED -Dsun.java2d.uiScale.enabled=false -Xmx50331648 -Xms16777216 -Dlax.debug.level=4 -Dlax.debug.all=true -Djdk.util.zip.disableZip64ExtraFieldValidation=true
CLASSPATH:/tmp/install.dir.38823/InstallerData:/tmp/install.dir.38823/InstallerData/installer.zip:

========= Forking JAVA =============================================

```
0 Kudos
Reply