Re: ZLG communication problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: ZLG communication problem

3,447 Views
yang_jacky
Contributor III
hello MichaIH:

I want to ask a question, that Is CANFD tool support available in freeMaster now?"
0 Kudos
Reply
3 Replies

3,425 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I will move your post to a new topic and will answer there shortly.

Thanks,
Michal

0 Kudos
Reply

3,417 Views
MichalH
NXP Apps Support
NXP Apps Support

Hello:

CAN FD is currently being added, with initial support for ZLG, Kvaser and IXXAT devices. We plan to include it in the next 3.2.6 release during October.

The FreeMASTER driver for MCU already enables to configure the CAN-FD option and we even have an example application adapted for CAN-FD (such as the FRDM-MCXN947 app). Of course, this work is now unusable until the FreeMASTER application will support this communication.

If you are interested to test the prototype version of the CAN plug-in, reach out to me at [email protected].

Regards,
Michal

0 Kudos
Reply

3,421 Views
yang_jacky
Contributor III
Ok, thank you
0 Kudos
Reply