Hello,
Let's use the other thread to discuss the FreeMASTER performance issue that you have reported earlier.
You again do not specify the issue any closer. Now you mention also some S32K crashing without being anyhow specific. You will need to describe the issue in better details. Describe the application and problem symptoms that you observe.
Regards,
Michal
Hello,
FreeMASTER does not block - with serial line it uses either polling or interrupt-driven mechanism as configured in freemaster_cfg.h.
The crash should not be related to FreeMASTER. Perhaps only ifs project is set up to read a memory/variable on an undefined address etc. You can try to reduce the FreeMASTER project to a bare minimum with a start/stop variable only in the Watch View and with the HTML control page removed.
What kind of crash is it (hardfault?). Can you track the origin of the fault?
Do you use the NXP motor control demo or your own solution?
Regards,
Michal
FreeMASTER should not cause program runaways etc. If an improper variable would be sampled by FreeMASTER at invalid address, you would be getting a hardfault. Code runaway is typically caused by stack overflow, corrupting stack by modifying deleted variables etc.
FreeMASTER driver is no magic - it is quite simple handler of serial communication and a protocol interpreter.
I recommend to increase a stack size and monitor its usage. I'm afraid you will need to debug and trace the issue down to locate the real problem.
Regards,
Michal