Freemaster connect fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freemaster connect fail

4,587件の閲覧回数
814420552
Contributor III

Dear all,

   when i connect  my board with openSDA, then open freeMaster tool,  boautrate is 115200, when click next step, it happeened the following error, pls  help me, only connect board and pc with USB line (openSDA)

pastedImage_1.png

0 件の賞賛
返信
3 返答(返信)

4,491件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hello,

it looks, that you want to connect via UART instead of the OpenSDA. For connection via UART, you need have the running Freemaster in the board too. 

If you want to use only OpenSDA, please select the highlited option in wizard.

pastedImage_1.png

And after then, you will see options of the debug connections:

pastedImage_2.png

Best regards,

Vilem

0 件の賞賛
返信

4,491件の閲覧回数
814420552
Contributor III

hello, whether has some manual or document for how to use this tool(FreeMaster)? 

wish you can share it to me, thanks very much!!

0 件の賞賛
返信

4,491件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hello,

you can find all documents on the NXP web page: FreeMASTER Run-Time Debugging Tool | NXP 

Best regards,

Vilem

0 件の賞賛
返信