Deinstalltion FreeMaster 3.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deinstalltion FreeMaster 3.2

Jump to solution
2,742 Views
peta
Contributor I

Hello,

My installation of FreeMaster 3.2 was aborted. When reinstalling, I get an error message that the software is already present and an upgrade is not possible. How can I install the software again?

Peter

0 Kudos
Reply
1 Solution
2,720 Views
iulian_stan
NXP Employee
NXP Employee

Just to make sure - are you able to access hidden folders on your system ? By default, Zero G Registry is a hidden folder and may not show up in explorer/search window for users with limited privileges.

If you have admin rights on your PC, could you update system options to show hidden folders and try searching for the folder/file on your system disk.

A few additional questions:

  • Are there any remaining files from the previous installation on you disk (ex: C:/NXP/FreeMASTER 3.2/) ?
  • Does FreeMASTER 3.2 shows up in Program and Features under Control Panel ?

 

View solution in original post

0 Kudos
Reply
4 Replies
2,728 Views
peta
Contributor I

Hi julian,
thanks for the quick replay.
I don´t have this folder or the file on my notebook.

Kind regards
Peter

0 Kudos
Reply
2,721 Views
iulian_stan
NXP Employee
NXP Employee

Just to make sure - are you able to access hidden folders on your system ? By default, Zero G Registry is a hidden folder and may not show up in explorer/search window for users with limited privileges.

If you have admin rights on your PC, could you update system options to show hidden folders and try searching for the folder/file on your system disk.

A few additional questions:

  • Are there any remaining files from the previous installation on you disk (ex: C:/NXP/FreeMASTER 3.2/) ?
  • Does FreeMASTER 3.2 shows up in Program and Features under Control Panel ?

 

0 Kudos
Reply
2,716 Views
peta
Contributor I
Okay, I could fix it. Installation is done, thanks for your help. Best regards Peter
0 Kudos
Reply
2,732 Views
iulian_stan
NXP Employee
NXP Employee

Hi Peter,

Could you check this post and let us know if that works for you.

King regards,
Iulian

0 Kudos
Reply