Yocto project building is failed. ERROR:pango_1.46.2.bb:do_compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto project building is failed. ERROR:pango_1.46.2.bb:do_compile

1,219 Views
HT_MOB
Contributor II

I'm trying to implement a Yocto-generated image on i.MX 8M PLUS.

Therefore, the following image is built in Yocto project, but an error occurred. Do you know how to resolve this error?

Host PC: ubuntu16.04
Rev: LF5.10.9_1.0.0
MACHINE: imx8mpevk
DISTRO: fsl-imx-wayland
image: imx-image-full

↓ Details of the error

ERROR: Task (virtual: native: /home/jrcm/source/NXP_iMX8MPLUS/imx-yocto-bsp_v2/sources/poky/meta/recipes-graphics/pango/pango_1.46.2.bb:do_compile) failed with exit code '1'

0 Kudos
Reply
0 Replies