Hi @xinliwang !
Yeah, I already had this problem. I don't know the exact reason but I have several hypothesis.
- First, check that the IPv4 adress of your netopeer2-cli belongs to same sub-network as your netopeer2-server.
- Then, plug an Ethernet cable on the interface eno0 (MAC0) of your board (not the interfaces of the switch swp0 to swp3).
- Finally, reboot your board.
If you follow these instructions, it is supposed to work. You don't need to run netopeer2-server when your board has boot. Indeed, netopeer2-server is running when your board is booting. You can check that here : /etc/init.d/S91netoper2-server.
Normaly, if you have the lastest version of openil running on your board, sysrepod,sysrepo-plugind, sysrepo-tsn and netopeer2-server are already installed on your board. You can check it by searching on the file system of the board. For exemple on /ect/sysrepo.
I hope this answer will solve your problem. If it doesn't solve the problem, let me know.
Finally I have a question for you. Do you know how can I configure a VLAN interface using NETCONF/YANG protocole ? I can't see the good file on this Github...
sysrepo-tsn/Instances at master · openil/sysrepo-tsn · GitHub
Sincerely,
asanson