GPT timer lower count ISR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPT timer lower count ISR

2,084 Views
manuel_iglesias
Contributor II

I am trying to generate a GPT interrupt as fast as possible, using the example code, the GPT clock source is 62.5MHz but I can only get an interrupt every 1us (not exactly as comparison count is 62 or 63 . If I specify a smaller compare value, the interrupt didn't seem to be triggering. Does anyone know if there is a limitation here?


Can it be possible to use a high speed internal clock, I have tried to change to the high frequency clock without seeing a difference. I might be missing some synchronization or something while trying to enable it.

I will appreciate any help,

Thanks,

Tags (1)
0 Kudos
Reply
1 Reply

1,996 Views
lucas_cao
NXP Employee
NXP Employee

Hello,

May I know What did you do during the interruption process and how to get the signal of the interrupt has been generated?

Lucas Cao

0 Kudos
Reply