Add librosa in Yocto project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add librosa in Yocto project

1,851件の閲覧回数
Joly
Contributor I

Hello,

I have a Yocto project in which I have to include Python a specific python library imported by a script (librosa)

I added it in my image and created a recipe for it with devtool.

When I build my image, it the requires further dependencies for this new library but I'm facing some problems:

- when I add the missing dependencies with devtool, it can fail (ie. parsing failure on adding numba)

- adding libraries with '_' in their name is not possible straightforward, it requires to replace with another character in the recipe name (ie. lazy_loader, typing_extensions) which can lead to compilation errors when lauching bitbake librosa.

 

I'm a complete beginner in Yocto.

Has someone already done it ?

Is there another way I could embed librosa in my soft ?

 

Thanks for any help

 

Alexandre

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)