KIT-HGDRONEK66 different motors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KIT-HGDRONEK66 different motors

ソリューションへジャンプ
9,609件の閲覧回数
rubenS
Contributor I

Hi, I recently bought the KIT-HGDRONEK66 and I wanted to build it following the gitbook. In the gitbook they use BLDC brushless motors 2212 920 kV but in my package there are flycat i-rotor 5010-750kv.

I couldn't find any website where these motors are in this kit.

Did I get the wrong motors or do these also work? The packing list says that I've got the right motors.

ラベル(1)
1 解決策
9,598件の閲覧回数
GeraldP
NXP Employee
NXP Employee

Lucky you! You got a kit with the new motors / bigger propellers that have better performance. We have not updated our gitbook yet. Sorry for that.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
9,599件の閲覧回数
GeraldP
NXP Employee
NXP Employee

Lucky you! You got a kit with the new motors / bigger propellers that have better performance. We have not updated our gitbook yet. Sorry for that.

0 件の賞賛
返信
9,591件の閲覧回数
rubenS
Contributor I

ok thank you. 

Is it necessary to wait for the gitbook or is it more or less the same?

0 件の賞賛
返信
9,580件の閲覧回数
GeraldP
NXP Employee
NXP Employee

Mounting and connection to ESC's is the same. Also motor spin direction is the same.

0 件の賞賛
返信
9,467件の閲覧回数
PGB123
Contributor II

I got the same motors but was given 4 counterclockwise threaded propeller hubs instead of the 2 counter and 2 clockwise. Was that a mistake in packaging or am I missing something?  

0 件の賞賛
返信
7,927件の閲覧回数
ArianRF
Contributor IV

Hi @PGB123 @GeraldP 

I got the same motors that look all counter clock wise. Did you figure out how to make 2 of them clockwise?

 

Cheers,

Nader

タグ(1)
0 件の賞賛
返信
7,904件の閲覧回数
iaingalloway
NXP Employee
NXP Employee

The motors are now all CCW (same direction) threads. Just ensure they are tightened well so they don't unscrew.

7,897件の閲覧回数
ArianRF
Contributor IV

Thanks Iain.

I am putting your comments from a different thread here for others  who have the same questions.

"They SPIN CW and CCW, but the screw thread is all in one direction.

The rotation direction is controlled CW/CCW by swapping any two of the three wires."

 

Cheers,

Nader