how fast the two-way communication between MWCT1013AVLH and MWPR1516 up to ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how fast the two-way communication between MWCT1013AVLH and MWPR1516 up to ?

1,085件の閲覧回数
wesleyxie
Contributor III

Hi, NXP

we are going to design a wireless Qi charging TX/RX module, plan to use MWCT1013AVLH and MWPR1516.

in this system, we also want to stream CAN data from Tx module (MWCT1013AVLH) to Rx module (MWPR1516).

so I wonder how fast the two-way communication between MWCT1013AVLH and  MWPR1516 up to ?

is it fast enough to stream CAN data ?

and, is that two-way communication able to exchange user data ?

thanks

/WX

0 件の賞賛
返信
0 返答(返信)