controller DSP56F803

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

controller DSP56F803

3,226件の閲覧回数
Mohamed512
Contributor I

I have one DSP56F803 content program and another one is blink ,

- i want to copy the program from the first to second .

- i want to test the first is ok or no . 

what are hardware and software  i will need to do two operations ?

 

the best regards

 

Mohamed Sayed

0 件の賞賛
返信
4 返答(返信)

3,191件の閲覧回数
Mohamed512
Contributor I

Thank you for rapid reply .

Are there manual for flash –over-jtag software ?

i need more details about these commands .

If firmware not protected , Do I use the same software ?

The best regards

 

Mohamed

0 件の賞賛
返信

3,214件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

In order to protect firmware IP, we do not have the dedicated tools to copy the code to a file.

But I think you can use flashOverJtag.exe tools to read the binary code to a file, but the flashOverJtag.exe tools is very old(I suppose that the tools was released in 2000 year), you have to get an old PC which has 25 pin parallel port and supports DSC OS. The flashOverJtag.exe tools only support DOS environment.

 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

3,147件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the user manual of FlashOverJtag.exe tools.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

3,211件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You can download flashoverjtag from the website:

https://community.nxp.com/t5/Digital-Signal-Controllers/Flash-over-jtag-exe-tools/ta-p/1115456

 

BR

XiangJun Rong

0 件の賞賛
返信