controller DSP56F803

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

controller DSP56F803

2,350 次查看
Mohamed512
Contributor I

I have one DSP56F803 content program and another one is blink ,

- i want to copy the program from the first to second .

- i want to test the first is ok or no . 

what are hardware and software  i will need to do two operations ?

 

the best regards

 

Mohamed Sayed

0 项奖励
回复
4 回复数

2,315 次查看
Mohamed512
Contributor I

Thank you for rapid reply .

Are there manual for flash –over-jtag software ?

i need more details about these commands .

If firmware not protected , Do I use the same software ?

The best regards

 

Mohamed

0 项奖励
回复

2,338 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

In order to protect firmware IP, we do not have the dedicated tools to copy the code to a file.

But I think you can use flashOverJtag.exe tools to read the binary code to a file, but the flashOverJtag.exe tools is very old(I suppose that the tools was released in 2000 year), you have to get an old PC which has 25 pin parallel port and supports DSC OS. The flashOverJtag.exe tools only support DOS environment.

 

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

2,271 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the user manual of FlashOverJtag.exe tools.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

2,335 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

You can download flashoverjtag from the website:

https://community.nxp.com/t5/Digital-Signal-Controllers/Flash-over-jtag-exe-tools/ta-p/1115456

 

BR

XiangJun Rong

0 项奖励
回复