about:twr-56f8400 ---AN5014SW, can't build the example project success in CW 10.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about:twr-56f8400 ---AN5014SW, can't build the example project success in CW 10.5

2,906 Views
kgz
Contributor I

I download “AN5014SW.zip” in freescale website----Software to accompany application note AN5014

and unzip to folder “PMSM_SNSLESS_DSC”.

Then I import project “56F84xxx_TWR--/56F84789_MID_SAC_TWR” into CW10.5.

But I meet some problems. Pls help me to deal with them.

 


22669_22669.jpg临时1.jpg

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,646 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, KeGang,

I use CodeWarrior for MCU ver10.6 to compile the project, I have not any problem. Maybe the different version of CW for mcu tools leads to the issue. I suggest you use CW for mcu ver10.6, you can uninstall the ver10.5 of CW for mcu tools, and install the ver10.6.

Hope it can help you.

BR

Xiangjun Rong

0 Kudos
Reply

2,646 Views
kgz
Contributor I

Dear Xiangjun:

I meet a special problem. I can compile this project in CW10.6 in a 32bit Win7 OS. But in another computer with 64bit Win7 OS, also in CW10.6, It is same failure.

kegang

to freescale.jpg

0 Kudos
Reply

2,646 Views
johnlwinters
NXP Employee
NXP Employee

Try doing a clean on project?

0 Kudos
Reply