Wrong data message on SC18IM700

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wrong data message on SC18IM700

1,201件の閲覧回数
ruben_marques
Contributor I

Hi there,


I'm having a issue regarding some UART messages on SC18IM700.

I send, for example, the folowed message by UART:


0x53 0x40 0x02 0x55 0x55 0x50 0x52 0x0A 0x50


That message works properly. I have a PCF controller with 0x40 address. I receive 0xF0 and can see the outputs changed.

In fact, all kind of messages works well, unless when I need to send a 0xFF (eg: 0x53 0x40 0x02 0xFF 0xFF 0x50 0x52 0x0A 0x50). In that case the SC18IM700 doesn't send anything by I2C (I confermed by osciloscope, and nothing hapens on I2C lines).


Any ideas?

Cumps,

Rúben Marques

ラベル(1)
0 件の賞賛
返信
0 返答(返信)