What jtag interface would you recommend for the 56F8367 running the most recent Codewarrior for Eclipse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What jtag interface would you recommend for the 56F8367 running the most recent Codewarrior for Eclipse

1,875件の閲覧回数
LesleyF
Contributor I

We are evaluating the Eclipse Codewarrior.  What type of JTAG interface is best for this?

Where should we order this?  From NXP or from somewhere else?

 

Thanks!

 

Lesley Freed

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,757件の閲覧回数
dynapb
Contributor IV

Hi Lesley

I use the USB Tap from NXP and it works ok.

At the moment the codeset is small and debug is slow on Eclipse compared to Classic CW.  I think it is probably just the overhead of Eclipse.

Pete

0 件の賞賛
返信

1,757件の閲覧回数
charliewu
NXP Employee
NXP Employee

Both USB Tap and PnE Universal-Multilink are recomended. But seems Multilink may be  a little bit faster during the debug session.

0 件の賞賛
返信