What jtag interface would you recommend for the 56F8367 running the most recent Codewarrior for Eclipse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What jtag interface would you recommend for the 56F8367 running the most recent Codewarrior for Eclipse

1,824 Views
LesleyF
Contributor I

We are evaluating the Eclipse Codewarrior.  What type of JTAG interface is best for this?

Where should we order this?  From NXP or from somewhere else?

 

Thanks!

 

Lesley Freed

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,706 Views
dynapb
Contributor IV

Hi Lesley

I use the USB Tap from NXP and it works ok.

At the moment the codeset is small and debug is slow on Eclipse compared to Classic CW.  I think it is probably just the overhead of Eclipse.

Pete

0 Kudos
Reply

1,706 Views
charliewu
NXP Employee
NXP Employee

Both USB Tap and PnE Universal-Multilink are recomended. But seems Multilink may be  a little bit faster during the debug session.

0 Kudos
Reply