The problem of MC56F8006's self-reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem of MC56F8006's self-reset

2,701 Views
khalil001
Contributor II

I am using the MC56F8006's demo, and I have a problem about the self-reset.

 

I have downloaded a program for generating a PWM wave.

After I debugged it , when I started the demo, the MC56F8006 always self-reset after a few times.

 

Please tell me what's the reason.

 

Thank you very much!

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,508 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls check if you disable the watchdog.

BR

Xiangjun Rong

0 Kudos
Reply

2,508 Views
khalil001
Contributor II

Thanks for your reply.

the watchdog is disabled.

0 Kudos
Reply

2,508 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you run MC56F8006 in standalong mode without debug, does the MC56F8006 reset event happens?

BR

XiangJun Rong

0 Kudos
Reply

2,508 Views
khalil001
Contributor II

It's first time for me to use DSC.

so could I ask you how to run MC56F8006 in standalong mode with out debug?

Thank you very much.

0 Kudos
Reply

2,508 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The standalong mode means that the MC56F8006 runs after power on. You just need to power on so that the DSC can run, it is okay.

BR

XiangJun Rong

0 Kudos
Reply