Switch audio input to SPDIF on a SAF77 chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Switch audio input to SPDIF on a SAF77 chip

2,886件の閲覧回数
Nickldio
Contributor I

Hello,

I am trying to switch the audio input on my car radio to SPDIF. The radio has the SAF7730HV chip on it, and I'm struggling to find any documentation on it. However, I found one for the SAF7741. Are they similar enough to work with that instead? I'm looking for the I2C registers to switch the input to SPDIF.

Does anyone have an idea how to achieve this? Is there documentation on NXP's I2C commands for similar chips, assuming they may be the same for mine?

 

Thanks

0 件の賞賛
返信
2 返答(返信)

2,370件の閲覧回数
efefurkan
Contributor I

Hello if you have saf7741 i2c memory map or datasheet different.

Could you share it ?

I am trying some changes on my radio which is using saf7741.

Thank you .

0 件の賞賛
返信

2,842件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

It appears that the docs related to SAF7730HV are confidential, pls contact NXP sales or FAE to apply for it.

BR

XiangJun Rong

0 件の賞賛
返信