SGTL5000: HP_VGND and mic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000: HP_VGND and mic

3,349件の閲覧回数
UweA
Contributor I

Hello!

I want to use the headset port with HP_VGND. In figure 19("Typical Application Schematic") it is shown that the mic is using GND. My 4 pin headset jack has only one pin for ground so I would get a shortcut of HP_VGND and GND if I would use it in such way. My question is: Is it possible(and reasonable) to use HP_VGND also for the mic?

-Uwe

0 件の賞賛
返信
3 返答(返信)

3,318件の閲覧回数
UweA
Contributor I

Hi,

@xiangjun_rongThank you for the schematics.
I know that it is a bad idea to connect HP_VGND to GND. But my question was (and is): Can I use HP_VGND(instead of GND) also for the headset mic?

KR,
Uwe

0 件の賞賛
返信

3,295件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the HP_VGND is only for the headphone instead of mic.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

3,335件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the EVK board schematics, pls check the connection.

I do not think you can connect the HP_VGND to GND directly, pls refer to the Note:

HP_VGND Note: Do not connect HP_VGND to system ground, even when unused. This is a virtual ground (DC voltage) that should never connect to an actual “0 Volt ground”. Use the widest, shortest trace possible for the HP_VGND.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信