PT3816EVM DIP settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PT3816EVM DIP settings

2,050件の閲覧回数
gmuhafeez
Contributor I

Hi, 


We are using the PTN3816EVM and giving input of 5k 60Hz signal with 5 meter DP cable at the Host and 5 meter DP cable at the Monitor end. We see that Using EVM brd and 5 meter cables Display doesn't come up. But we used one Cablematters Redriver(https://www.amazon.in/Cable-Matters-DisplayPort-Amplifier-Resolution/dp/B07D949F59) Link above works with 5 meter at the input and 5 meter at the output works. So Is there any setting we need to change at the DIP ? Can you please help us with it ? 


Thanks, 
Muhafeez

0 件の賞賛
返信
2 返答(返信)

2,040件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Suggest don't use the DP cable longer than 3meters.

 

0 件の賞賛
返信

2,034件の閲覧回数
gmuhafeez
Contributor I

Hi, 

Thanks for your response. 
Yes it comes up with the cable less than 3m. 
But My question is Does PT3816EVM doesn't support more than 3m ? 

Thanks, 
Muhafeez

0 件の賞賛
返信