PCA9698 ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9698 ERROR

1,590件の閲覧回数
shoujian_lv
Contributor I

HI

I use PCA9698 to solve the problem of insufficient IO port.

But there are problems in the use process:

I use the IO of pca9698 to control the digital switch(ADG1612),when the control port of the digital switch is not connected to the IO port of pca9698,i can control the IO as i want.

But when more than 4 control ports of the digital switch are  connected to the IO port of pca9698(these ports is in one register),and IO is configured as output,if set these ports(more than 4 ports) HIGH at same time,Configuration registers corresponding to these ports will be configure as input. In this case, it is invalid to configure IO as output.

タグ(1)
0 件の賞賛
返信
1 返信

1,511件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please also provide schematic!

0 件の賞賛
返信