PCA2131 RTC Behavior in Battery Backup Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA2131 RTC Behavior in Battery Backup Mode

1,095 Views
Kalpakg24
Contributor I

Hi,

We are using the PCA2131 RTC in our BMS design. When the VDD supply is powered at 3.3 V, the device operates as expected. However, when the RTC switches to battery backup mode (3 V coin cell connected to the BAT pin), the CLKOUT signal is not generated.

We would like to understand the behavior of the RTC in battery backup mode, specifically with respect to the availability of the CLKOUT and interrupt functionality. Our requirement is to have an interrupt generated in battery backup mode to wake up the BMS.

Please find the attached schematic for your reference.

Kalpakg24_0-1770890395473.png

 

 

Tags (2)
0 Kudos
Reply
1 Reply

1,040 Views
RafaR
NXP Employee
NXP Employee

Hello Kalpakg24

Sorry for the delay, it seems that your distributor has already contacted us internally and we are already providing support, we are going to continue using that medium, I hope there are no problems.

Have a great day and best of luck.

0 Kudos
Reply