NTB0104BQ-Q100X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTB0104BQ-Q100X

1,031 Views
beyondiv1986
Contributor I

Hi, I have a question about the use of the NTB0104BQ-Q100X.

From the NXP website, I know the  NTB0104BQ-Q100X is only suitable for the push-pull circult, and from the datasheet, It says   "the NTB0104-Q100 is not recommended for use in open-drain driver applications such as 1-Wire or I2C."

My question is "Could I use the NTB0104-Q100 just accept the output of  an open-drain driver , and transmit the signal to a   push-pull circult (only use for one direction: from OD to PP)"

THANKS! ^_^

0 Kudos
Reply
0 Replies