MC56F83000 development guide

cancel
Showing results for 
Search instead for 
Did you mean: 

MC56F83000 development guide

No ratings

MC56F83000 development guide

The MC56F83000 is the latest DSC family, which has new features the previous family does not have, I list them here so that customer can know the features before they develop application project.

1)USBTAP device is NOT supported

2)ROM bootloader is supported, so user can use blhost tools to download code in bootloader mode after Reset

3)Write configuration field so that the MC56F83xxx knows whether it starts from application code in Flash or bootloader code 4)Add #pragma macro as prefix before ISR

Attachments
Version history
Last update:
‎11-15-2021 08:49 PM
Updated by: