MC56F8037 I2C rise time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8037 I2C rise time

1,387件の閲覧回数
EngHuiPeng
NXP Employee
NXP Employee

Would like to check whether there is any tolerance/allowance on the I2C rise time of the DSC. Customer informed that their I2C rise time is approx ~1.744uS which exceeds the max 1uS rise time recommendation but the communication have no issue. 

 

Thanks.

 

Regards,

Hui Peng

ラベル(1)
0 件の賞賛
返信
1 返信

1,167件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Hui,

The data sheet specifies that the maximum rising time for both SCL and SDA is 1uS in standard mode, but I think it is okay if the I2C module works fine even if the rising time is 1.7uS.

Hope it can help you

B R

Xiangjun Rong

0 件の賞賛
返信