Yes I tried those instructions and using that project (mine is C:\Freescale\CW_SC_3850_v10.7.2\SC\StarCore_Support\I2CBoot\MSC815x-MSC825x)
The problem is using the project and USB TAP as the JTAG., I get:
!ENTRY com.freescale.core.debugger.cdt 4 16777218 2019-02-20 08:53:39.038
!MESSAGE Failed to resume target process., CCSProtocolPlugin : Error writing memory
Unless I set JTAG as a ISS connection type… which will not allow map to the I2C or RCW registers since it’s Instruction Simulation..
How do I get the projec to use the USB TAP as the JTAG connectin?