How to port a quickstart for DSC 2.5 generated project from classic to eclipse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to port a quickstart for DSC 2.5 generated project from classic to eclipse

2,704 Views
ankur_kala
NXP Employee
NXP Employee

Hi,

 

we have a project developed on CW8.3 using Quickstart 2.5 based on 56F8006 device. Now we need to port it on CW10.6. Is there any simple means to do that. I see that the Quickstart2.5 stationary just has *.mcp (project file for classic codewarrior) support.

Labels (1)
0 Kudos
Reply
3 Replies

2,404 Views
johnlwinters
NXP Employee
NXP Employee

CodeWarrior projects for CW8.3 for DSC may be imported using CW10.6 for MCU.

The fact that it is a QuickStart project may or may not introduce complications, as I have not attempted to convert such projects.

Have you tried the import feature of CW10.6 to import the CW8.3 for DSC project?

0 Kudos
Reply

2,405 Views
ankur_kala
NXP Employee
NXP Employee

Hi John,

Yes I tried importing it, but the improted code generated errors for dependencies of appconfig that gets generated by Quickstart.

Regards,

Ankur

0 Kudos
Reply

2,405 Views
johnlwinters
NXP Employee
NXP Employee

For support on this tool, you need to contact ROsnov engineers directly.

0 Kudos
Reply