Example project for MC56F84789 data flash erasing and writing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example project for MC56F84789 data flash erasing and writing

2,704件の閲覧回数
johnlwinters
NXP Employee
NXP Employee


This example, attached as an export from CW10.5 for MCU (with DSC option selected at install) (with first published update as of Nov 22, 2013 included), show how data flash can be erased and used to store information, and then later erased.

Processor Expert was used to generate the code.

The drivers are totally visible in the project as source code and may be used as a model for customer code to do similar functions.

 

The device used in this example is MC56F84789.

 

To use this example code, save the zip file on your disk.

Unzip the file.

 

Then use the import function of CodeWarrior 10.5 for MCU's to import the project as an existing project.

 

It was exported as a file system with complete structure preserved.

Original Attachment has been moved to: 84789DataFlash.zip

ラベル(1)
0 件の賞賛
返信
0 返答(返信)