Element definition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Element definition

6,593 Views
ineedit89
Contributor II

Good day. On the tracking generator board there is a radio element with smd code 7017G 5124 P1116. Please tell me is it your boardband gain block BGA7017. Also tell me if you have a radio element with the smd code SK17 1343, if yes what it is  a element? With respect and best wishes to you and thanks for Your answer!


					
				
			
			
				
			
			
				
			
			
			
			
			
			
		
0 Kudos
Reply
5 Replies

6,448 Views
ineedit89
Contributor II

thank You for all)

0 Kudos
Reply

6,448 Views
ineedit89
Contributor II

Good afternoon Pavel. Your information halped me a lot. Thank you very mach!!! One more question. You said that NPX is not manufactured BGA7017, but i have a pdf with this add and Your logo stand there. Link at the end of the appeal. Please explain this for me. Xan i contact You in Russian? With best wishes! 

https://nanopdf.com/download/bga7017-30-mhz-to-6000-mhz-broadband-gain-block_pdf

0 Kudos
Reply

6,448 Views
LPP
NXP Employee
NXP Employee

The aim of community forum is to share knowledge among the designers. I could  understand Russian but our general rule is to provide support only in English.

https://www.nxp.com/wcm_documents/products/related/nxp_rf_manual_16th_edition.pdf
BGA7017 was developed and it has been announced to be released in Q4 2012.
Though, It did not happen. I don't know the reason why.

At the moment, I was not able to find any related information in available repositories and our Product Change Notification database.

Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

6,448 Views
LPP
NXP Employee
NXP Employee

BGA7017 hasn't been ever released by NXP. It might be a Mimix/Macom device:

https://datasheet.ciiva.com/15200/getdatasheetpartid-622008-15200830.pdf

>smd code SK17
SKYWORKS SKY65017-70LF
https://www.mouser.com/ds/2/472/SKY65017_70LF_200528G-1131841.pdf


Have a great day,
Pavel

NXP TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

6,448 Views
ineedit89
Contributor II

Добрый день, Павел. Могу я могу обращаться к Вам на русском? Ваша

информация мне очень помогла спасибо вам большое!!! Я закрою тему на днях.

Но у меня ест к Вам еще 1 вопрос. Вы сказалаи что NXP не изготавливала

BGA7017 но у меня есть pdf с этим элементом и там стоит Ваш логотип. фаил

прилагаю. Объясните пожалуйста это. Если запрос сделанный на русском Вам не

понятен укажите это и я перепишу на английском.

пт, 22 мар. 2019 г. в 14:31, LPP <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Element definition

reply from LPP

<https://community.nxp.com/people/LPP?et=watches.email.thread> in *Digital

Signal Controllers* - View the full discussion

<https://community.nxp.com/message/1128895?commentID=1128895&et=watches.email.thread#comment-1128895>

0 Kudos
Reply